Drop-In Replacements for Discontinued Linear Transducers
If you’re looking for drop-in replacements for discontinued linear transducers, look no further than Balluff.
We know it’s a hassle to remove existing connector cables and replace them with a different type just so you can install one of the newer-style transducers. Buying an extra cost adapter cable is no answer either – it just adds another point for potential contact failure. That’s why Balluff is offering Micropulse® transducers with backward-compatible legacy connectors.
All Micropulse® transducers come standard with patented autotuning electronics for use with the existing magnet in the hydraulic cylinder. That means you don’t have to open up the cylinder to change the magnet – even if it’s not from Balluff. And Micropulse® transducers are built tough to hold up in demanding industrial applications. They’re as rugged electrically as they are mechanically.
So next time you need to replace a transducer, make it easy on yourself. With Micropulse® from Balluff, you’ll need to replace only the transducer. See how easy it is by contacting Balluff today for expert cross-reference assistance.
You can get a preview of Balluff’s drop-in replacements by clicking on one of the informative packets below.