english
Home  |  Products  |  Applications  |  Industry  |  Downloads  |  Sales + Service  |  News  |  Search  |  Company  |  Contact Us  |  MyList
Search

Content Control of Plastic Bottles
Verify package contents and fill level.


 

A long range shielded capacitive sensor is mounted closely to the plastic bottle packages on the conveyor belt. The sensor performs two duties in its function as post quality inspection on this packaging line. First, the Balluff BCS capacitive sensor detects accurately if a certain fill level in the bottle has been reached. Secondly, it detects if there is a plastic bottle in the carton package at all. If neither, the fill level nor the contents is present, the sensor gives a signal to the PLC.

Recommended sensors: BCS D50OO02-YPC25C-EV02 or BCS M30B4M3-PPM20C-EP02


 
1-800-543-8390        http://www.balluff.com/us