Tool coding
Tool coding

The right tool at the right time at the right place

The transfer of tool parameters from the pre-setter such as offsets, tool number, diameter and length to the CNC control ensures optimum tool use and high machine availability. Downtime monitoring and asset management concepts prevent unproductive idling, incorrect assignments and tools that are missing or not sharpened according to schedule.

Tool ID solutions read the current status on the tool and document all data. This enables forecasting for future use. And the quality and efficiency of the production process therefore improve while costs drop and efficiency increases.

With Industrial RFID, you always have the right data in the right place at the right time. And you are best positioned for Industry 4.0.

Application examples

  • Tool presetting

    Reliable data storage of tool data in the tool holder

    The solution

    The tool setting device with integrated RFID read/write unit automatically detects the loaded tool based on the tool number. After that, it writes the measured actual tool parameters to the RFID chip on the tool holder.

    The features

    • Automatically detect tool
    • Write actual tool parameters to RFID chip on the tool holder
    Metal machining, adjusting tools
    Find suitable products Download

    Contact us

    Have any questions? Please give us a call or send us an email. We look forward to hearing from you.

  • Documenting tool data

    Parameters on RFID chip make the tool usable at any time

    The solution

    The unique documentation of all parameters via RFID chip on the tool holder is very reliable. This is because the tool can remain in storage unused for a long time without the data getting lost. If necessary, it can be reused immediately.

    The features

    • Unique documentation of all parameters
    • Data do not get lost
    • Tool, if currently unused, can be reused at any time
    Metal machining, documenting tool data
    Find suitable products Download

    Contact us

    Have any questions? Please give us a call or send us an email. We look forward to hearing from you.

  • Error Free data entry to the CNC controller

    Transfer tool data to the controller in real time

    The solution

    Before or during introduction of the tool into the tool spindle, the RFID chip reads in the actual tool parameters. Alternatively, the data can also be read in if tools are loaded into tool storage – chain or magazine.

    With both options, all current tool data are transferred in real time to the CNC control.

    The features

    • Read in tool parameters when the tool is introduced or when the tools are loaded into tool storage
    • Transfer tool data in real time to CNC control
    Metal machining, informing CNC control
    Find suitable products Download

    Contact us

    Have any questions? Please give us a call or send us an email. We look forward to hearing from you.

  • Organizing data mapping

    Mapping for your requirements

    The solution

    Decentralized data storage on the RFID chip has the advantage that the tool parameters are always and independently available from the central server.

    As the user, you define the extent to which these parameters are stored according to your requirements.

    Especially important here: So-called data mapping, which is the storage address organization coordinated between adjusting device, storage management and machine tool. There are various mappings depending on the manufacturer. You can readily use the Balluff mapping suggestion if applicable.

    Metal machining, organizing data mapping
    Find suitable products Download

    Contact us

    Have any questions? Please give us a call or send us an email. We look forward to hearing from you.