Basics of Automation > Fundamentals of Automation > Resolution, non-linearity, accuracy

What resolution, non-linearity and accuracy mean

Did you know that the resolution, non-linearity and accuracy are among the most important features of a measuring sensor system? These vary significantly depending on the application requirement and the measuring principle. We will explain the terms now.

Basics of Automation – Resolution
Resolution
Basics of Automation – Non-linearity
Linearity deviation

Resolution is the smallest possible physical change which the measuring system can detect.

Non-linearity is the maximum deviation from a straight line that connects the zero point of a measuring range with the end point/ full scale. There is a linear relationship between the position or distance traveled and the output signal.

Resolution – High precision
High precision, poor accuracy
Resolution – Low precision
Low precision, good accuracy
Resolution – Accuracy
High precision + good accuracy = accuracy
Resolution – Multiple approach
Repeat accuracy

Accuracy is a measure of the agreement between measuring result and the true value for the measurand. Therefore high accuracy can only be achieved when the precision is high and the correctness is good. Another term in this connection is repeat accuracy. This results when a certain point is always approached under unchanged conditions.