Alternatives to fiber optics
Miniaturized photoelectric sensors offer a smaller bending radius and more focused light beam
![](/images-2/containers/assets/blog-amer/post-images/us-wp/bbp0390-moermond-alt-to-fiber-optics-blog-teaser.jpg/0ab548b0c734994d316a2268b43e1fed.jpg)
Reading Time: minutes
Fib fiber optic sensors may solve photoelectric applications with space restrictions, small part detection, high temperatures, or aggressive harsh environments. These sensors allow the electronics to be mounted out of harm’s way while focusing the light beam on a small target. The sensing tips can be manufactured in various housings for unique mounting requirements.
Fiber optic sensor basics
Fiber optic sensors require two components: a remote-mounted amplifier and the fiber optic cable(s). The amplifiers can be basic, with few features, or advanced, with many configurable options and digital displays. The fiber optic cables are made of either plastic or glass fibers, each with advantages and application-specific solutions.
Many applications, primarily those in the medical sciences and semiconductor industries, cannot be solved with fiber optic or miniature photoelectric sensors because they are physically too large to fit in the instruments. Additionally, the cables are typically not flexible enough to be routed through the instruments. Today, highly flexible and miniature sensors are being incorporated into other industries due to today’s demands for smaller machines and tools.
Miniaturized photoelectric sensors
MICROmote® sensors are miniaturized photoelectric sensors with separate amplifiers that are also available with various functionalities. Their highly flexible electric sensor cables make them a genuine technical alternative to conventional fiber optics. The photoelectric sensor heads have extraordinarily small dimensions, excellent technical characteristics, and outstanding flexibility for application-specific solutions.
Similar to fiber optic sensors, these micro-optic photoelectric sensors function as either a through-beam or diffuse sensor with comparable sensing ranges. Unlike fibers, the wired sensing heads are inherently bifurcated cables, so there is only one connection to the amplifier.
Differences from fiber optics
Unlike conventional fiber optic cables, there are no significant coupling losses, minimum bending radius, or cyclic bending stresses. The patented precision elements produce extremely small beam angles with sharply defined light spots, unlike standard fiber optics, where the beam angle is a function of the fiber geometry. Additional lenses must be used if the light beam of a fiber optic cable must be focused, which adds to the costs.
Detecting liquids with high water content
MICROmote® photoelectric sensors for water detection use a specific wavelength at which water absorbs more light. This significantly simplifies the detection of liquids with high water content using optical sensors. An ultra-compact design and powerful micro-optics allow for reliable use in capillary tubes where other sensing devices are stretched to their limits.
Detecting bubbles
These sensors can also be used as precision tube sensors for detecting bubbles. They use either light refraction or attenuation through the air or liquid column within the tube. They provide excellent detection for even the smallest air-to-liquid transitions and are reliable for all liquid types, even clear liquids.
In addition, these sensors are designed to detect free-floating microbubbles in transparent liquids. Microbubbles refer to little gas bubbles with dimensions smaller than the inside diameter of the tube. Uniform lighting is achieved in the liquid column using a concentrated arrangement of multiple light beams with uniform intensity distribution. Gas bubbles that move through this field induce a signal jump in the built-in photoelectric receiver elements.
Keywords
- Sensor technology
- Basics of automation
Author
Comment
Popular posts
The pros and cons of flush, non-flush and semi-flush mounting inductive sensors
Industrial sensing fundamentals – NPN vs PNP
How do I wire my 3-wire sensors?
The basic operating principle of an inductive proximity sensor
Contact form
Do you have any questions or suggestions? We are at your disposal.
Balluff GmbH
-
Schurwaldstraße 9
73765 Neuhausen a.d.F.