Products
Service & Support
Industries & Solutions
Company

Simulate machines and systems with the digital twin

Virtual commissioning made easy!

Imagine being able to create a digital representation of a physical object that replicates the behavior of that object. Regardless of whether it is a single machine or an entire production line, digital twins open up completely new possibilities for the industry. They help to plan commissioning, identify problems at an early stage and make well-founded decisions about planning, maintenance and optimization before the production systems or machines are actually available.

advantages_in_a_circle

Advantages of the digital twin

Faster commissioning of systems

advantages_in_a_circle

Better product quality

advantages_in_a_circle

Lower product development costs

advantages_in_a_circle

Shorter product development time

advantages_in_a_circle

Virtual commissioning in an industrial environment 

In order to meet the massive demands on performance, quality and costs as the level of automation increases, the use of virtual methods and tools is already essential in the development process (digital engineering) of industrial production systems. Virtual commissioning (VIBN) plays a central role here.


“Digital component twins offer virtual commissioners a detailed insight into the future performance of their systems. This advanced simulation tool reduces uncertainty, improves decision-making and ensures a smooth and predictable introduction of new technologies and processes.”

Dr. Philippe Komma, Product Manager


The digital twin at Balluff

The digital behavior model allows you to test how the machines behave in a virtual environment before they are even built. This saves time and money and ensures that the machines – whether stand-alone or part of a production line – work perfectly when they go into operation.

Digital twins in practice: Virtual commissioning of RFID sensors

A practical example of this technology is the digital twin of the Balluff BIS01E2 RFID read/write device. Here Balluff has created a component behavior model that models the communication between a controller and the RFID device.

To control the digital twins, a hardware-in-the-loop configuration can be set up which connects a digital twin of the RFID device to a physical programmable logic controller (PLC).

This setup means that control programs created during virtual commissioning can be used in the real commissioning phase with little or no adjustments.

Get in touch with us

Are you interested in digital twins in the context of virtual commissioning? Our experts will be happy to talk to you without obligation and advise you on the ways you can benefit from digital twins in principle and in specific applications.

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.

Contact us directly by phone: +32 (0)16 792970


Balluff Benelux

Hintham 117d
5246 AE Rosmalen, Netherlands

Please contact us:
[email protected]

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue