Products
Service & Support
Industries & Solutions
Company

Identify Failures Before They Happen: The Potential-Functional Curve

Bridging potential failure and functional failure in predictive maintenance

Tom Knauer
13 May 2026 | 09:50 Clock

Reading Time: minutes

The Potential-Functional (P-F) curve is often mentioned in condition monitoring and predictive maintenance discussions. It refers to the interval between the detection of a potential failure (P) and the occurrence of a functional failure (F).

Figure 1

The P-F curve is an illustrative generalization of what happens to an asset, machine or component as it ages, degrades, and eventually fails. It shows the different stages of an asset’s life, how machine failures progress, and how and when different symptoms emerge which might signal impending (or actual) failure.

The time scale in Fig. 1 is obviously exaggerated, and most assets operate for a lengthy period of time before failure starts to occur. The steepness of the failure portion of the curve can vary from asset to asset, but it generally follows the same pattern as shown in the diagram.

At first, performance degradation is minor and may not require significant action. As time progresses, the potential failure indicators become stronger and more easily detectable and the performance degradation becomes more severe, eventually ending in catastrophic failure.

The timeline is split into three domains:

Proactive domain

The failure is relatively far off (machine may still be new). Proactive activities include designing for reliability, precision installation & alignment and life cycle asset management. These can significantly extend the time until potential and functional failures occur.

Predictive domain

The failure may still be far off, but symptoms are emerging and offer (relatively) early warning signs. Timely action may be taken to prevent failure or replace failing equipment before catastrophic failure occurs.

Fault domain

The failure is occurring or inevitable, and symptoms indicate immediate action is needed to address the failure.

During these domains, different indicators/symptoms emerge. Ultrasonic, vibration and oil analysis often signal problems early; then temperature rise and noise emerge a bit later; and finally, parts come loose and more severe damage occurs. Depending on the asset, other indicators may be shown by activities including corrosion monitoring, motor current/power analysis and process parameter trending (e.g., flows, rates, pressures, temperatures, etc.).

By analyzing which symptoms of failure are likely to appear in the predictive domain for a given piece of equipment, you can determine which failure indicators to prioritize in your own condition monitoring and predictive maintenance discussions.

Keywords

  • Condition Monitoring

Did you like this post?

0

Share this post

Author

Tom Knauer

Tom Knauer

Tom Knauer has more than 30 years of industrial automation experience and has presented on condition monitoring and smart manufacturing/IIoT at the Automate Conference, the Assembly Show, IMTS and IME West.


0 Contributions

Comment

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue