Products
Service & Support
Industries & Solutions
Company

Choosing the Right Network Switches in Automotive Manufacturing

When to Use Unmanaged vs. Managed Industrial Ethernet Switches

John Takacs
13 May 2026 | 09:35 Clock

Reading Time: minutes

In the modern automotive manufacturing environment, data is every bit as critical as the steel, aluminum, plastics, and electronics that move through the plant every day. From robot weld cells to vision-guided assembly, from torque tools to press operations, reliable communication networks underpin nearly every production process. As manufacturers push toward greater automation, traceability, and system interoperability, understanding how to design the right industrial Ethernet architecture becomes a strategic advantage.

A foundational part of that architecture is the correct selection between unmanaged and managed Ethernet switches. Choosing the right type can greatly influence network stability, troubleshooting speed, long‑term scalability, and overall equipment effectiveness (OEE). Automotive manufacturers—who operate some of the most sophisticated, uptime‑critical environments in the world—stand to gain significantly from making the right switch choice for each application.

This article explores when to use unmanaged switches vs. managed switches, tailored specifically for automotive production systems. We’ll examine how each type works, their advantages, and use‑case examples tied to real‑world automotive scenarios.

The Role of Industrial Ethernet in Automotive Manufacturing

Industrial Ethernet has become the dominant communication backbone connecting PLCs, sensors, actuators, vision systems, welding controllers, robots, and more. Automotive plants rely on deterministic, high‑speed data flow to achieve cycle‑time precision and maintain the reliability expected from just‑in‑time (JIT) and just‑in‑sequence (JIS) production models. According to internal Balluff networking guides, Industrial Ethernet's robust physical layer and high‑speed throughput have driven exceptional global growth because it enables continuous communication down to the sensor and actuator level.

To support such networks, manufacturers have access to two primary categories of industrial switches: unmanaged and managed. While both provide fundamental connectivity, they differ greatly in capabilities and the scenarios where they should be applied.

What Are Unmanaged Switches?

Unmanaged switches provide essential Ethernet connectivity with no need for configuration. They are plug‑and‑play devices designed to forward network traffic transparently.

Key Characteristics:

  • Require no configuration and do not receive an IP address

  • Support auto‑negotiation for speed and duplex

  • Utilize standard Layer 2 forwarding, allowing all protocols to pass through

  • Offer ruggedized versions with IP67/IP20 housing for harsh environments

  • Automatically detect cable types through auto‑crossing, reducing wiring errors
    Many automotive environments still rely heavily on unmanaged switches for smaller machines or standalone equipment modules, particularly where cost and simplicity drive the decision.

What Are Managed Switches?     

Managed switches provide the same basic switching as unmanaged devices, but add powerful tools for network configuration, segmentation, diagnostics, and performance control.

  • VLANs

  • Diagnostic relays

  • IGMP snooping

  • Port mirroring

  • Monitoring & lockout

  • Spanning Tree Protocol (STP/RSTP)

  • Quality of Service (QoS)

  • Security features
    These features allow IT, controls, and maintenance teams to build resilient networks that can handle the complexity of modern automotive systems.

When to Use Managed Switches in Automotive Manufacturing

1. High‑Traffic Networks with Multicast (Vision Systems, AOIs, Robotics)

Automotive lines depend heavily on vision systems for:

  • Surface inspection

  • OCR/OCV

  • Presence/absence checks

  • Dimensional verification

Vision systems generate large volumes of multicast traffic. IGMP snooping, available only on managed switches, is essential to keep this traffic from overwhelming the network.

2. Large Production Lines with Long Runs and Many Nodes

Areas like body shop, underbody assembly, final assembly, and paint typically involve:

  • Dozens of robots

  • Hundreds of sensors

  • Multiple controllers

  • Safety and production networks in parallel

Managed switches enable:

  • VLAN segmentation

  • Prioritization of safety and critical traffic

  • Loop protection via RSTP

  • Predictive troubleshooting

Without this, a single broadcast storm can take down an entire zone.

3. Automotive Traceability Systems

Traceability is non‑negotiable in the industry. Systems must reliably handle:

  • RFID readers

  • Barcode cameras

  • Torque tools

  • Press monitoring systems

Managed switches provide the monitoring and diagnostic tools to maintain consistent plant‑wide connectivity.

4. Safety Networks

CIP Safety, Profisafe, and other safety protocols require:

  • Deterministic communication

  • Traffic isolation

  • Redundant paths

Managed switches provide QoS and path protection features that unmanaged switches cannot.

5. Remote Troubleshooting & Maintenance

Port monitoring, event logs, and mirrored traffic allow controls engineers to:

  • Capture packets

  • Diagnose intermittent issues

  • Identify cable breaks

  • Detect power loss

  • Find misconfigured devices

Automotive uptime targets often exceed 98–99%, making such diagnostics indispensable.

Unmanaged vs. Managed: Side‑by‑Side for Automotive

Requirement

Unmanaged Switch

Managed Switch

Low cost, simple machine wiring

✔ Ideal

Harsh environments (IP67)

✔ Available

✔ Available

No configuration needed

✔

Vision systems & multicast

✔ Required

Safety networks

✔ Required

Large‑scale body shop lines

✔

Troubleshooting & remote diagnostics

✔

VLAN separation (safety vs non‑safety)

✔

Future scalability

Moderate

Excellent

Keywords

  • RFID
  • Industrial network technology
  • IO-Link
  • Industry 4.0
  • Sensor technology
  • Robotik
  • The basics of automation
  • Industrielle Automatisierung
  • Trends in der Technologie
  • Connectivity
  • Message Queue Telemetry Transport (MQTT)
  • IoT
  • Condition Monitoring
  • distance measurement
  • flow measurement
  • Vision
  • Intralogistic
  • Inductive sensors

Did you like this post?

0

Share this post

Author

John Takacs

John Takacs

Global Key Account Manager Automotive OEM, 25+ years of Automation Sales, Account Management and large project management with Machine builders and Automotive Manufacturing


0 Contributions

Comment

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue