The delivery date can be documented and is within the period of 30 days
The return delivery is pre-announced by the customer and approved by Balluff.
The goods are in original packaging and hence in a resalable condition. Shrink wrapped or sealed products have to be in unopened condition.
The goods were purchased in the US.
It is catalog product.
The following materials are excluded from return shipment:
Non-returnable and non-cancellable products (KMAT)
Modifications (MOD)
Customized products
Safety products
Adhesive labels, generally products that have a limited shelf life
Without prior consultation with and approval by Balluff, a return is rejected.
Taking back and returing goods is always subject to reservation and without recognition of legal obligation. The final assessment is at the discretion of Balluff.
In the event of a wrong delivery or over-delivery caused by Balluff, we will refund 100% of the value of the goods.
For returns for other reasons with a net value of goods of less than 150,- € no credit note will be issued as a matter of principle.
For returns for other reasons with a net value of goods greater than 150,- € we refund the value of goods less 30% processing fee for the review and restocking expenses.
Transport and insurance costs are generally reimbursed only for goods under warranty and customer pre-announced via RMA.
Costs and expenses for returns of rejected goods is generally covered by the customer.