Products
Service & Support
Industries & Solutions
Career
Company

06.11.2024

Balluff at SPS trade show 2024

Straightforward and safe automation for the future

Balluff at SPS trade show 2024

Balluff will present its expanded network portfolio with new product lines at SPS. Picture: Balluff

At this year’s SPS, Balluff is set to present its expanded network portfolio and to give visitors a sneak peek at the new safety standard IO-Link Safety. The trade show booth will also feature new condition monitoring and machine vision products.  

Nuremberg, Germany — From November 12 through 14, the focus at the SPS (Smart Production Solutions) in Nuremberg, Germany will be on innovations in the automation industry — and the following question: How can automation solutions make industrial manufacturing more digital and more efficient? Balluff has an answer, presenting new network technology and sensors at the leading international trade show. The focus will be on products that reduce the complexity of production systems while increasing their level of performance and ensuring maximum security. 

A new take on safety  

Trade show visitors can also look forward to a sneak peek at the future of production system safety: as one of the leading providers of IO-Link solutions, Balluff will introduce IO-Link Safety at SPS — a new safety standard for industry. It allows machinery and production systems to be equipped with functional safety components such as safety doors and light curtains. IO-Link Safety ensures safe communication between safety devices and control systems, minimizing the risk to workers and machinery. Integrating IO-Link Safety into existing IO-Link systems is easy to implement thanks to standardized M12 connectors. 


The new network portfolio’s Black Line is characterized by its outstanding cost-effectiveness. The Silver Line features particularly robust network modules. Picture: Balluff

Network technology that meets every requirement 

The growing data traffic in industrial manufacturing makes high demands on network technology. Balluff combines high-performance networking components with IO-Link to ensure an optimal flow of information. At its SPS booth, the sensor and automation specialist will show its expanded network portfolio. Depending on the required performance and area of application, production system operators can choose between four different product lines: the Black Line forms the core of the new portfolio. It is very cost-effective and available in three performance categories (entry, standard, and advanced). The Silver Line is ideally suited for specialized applications that require a high level of robustness. Product lines for washdown environments and safety applications respectively complement the range. 


Upgrading condition monitoring 

Trade show visitors will also be able to take a look at the condition monitoring portfolio which offers particularly great potential for the automation of manufacturing processes. This is because condition monitoring sensors provide real-time data, for example from critical assemblies, making costly manual inspections unnecessary. One of the new products featured at the trade show booth: the condition monitoring sensor BCM Generation 2 which combines several monitoring functionalities and enables frequency-selective analysis. Compared to its predecessor, it features a significantly improved measurement performance in the detection of high-frequency phenomena. Thanks to the integrated intelligent data pre-processing capabilities, production system operators do not need any additional high-end evaluation units, reducing unnecessary data traffic. Another new BCM Gen 2 feature: a new mounting concept with just one screw. The small, round mounting surface makes it easy to retrofit the sensor, taking up only little space. 

The condition monitoring sensor BCM Gen 2 features a high measurement performance and can be installed using just one screw. Picture: Balluff


Beyond visible light 

In the area of machine vision, Balluff is set to present new models in the industrial camera BVS CA product family. They feature SWIR sensors (short-wave infrared) which use the short-wave infrared range of the light spectrum up to 1,700nm, reliably detecting things that are not visible or hard to detect for traditional cameras and the human eye. This makes them particularly suited for monitoring tasks in the semiconductor as well as the packaging and food industries. Another advantage: the cameras feature their own image memory and can pre-process and correct images using FPGA circuitry. The new SWIR models can be easily integrated into existing systems thanks to their compatibility with GigE Vision, USB3 Vision and GenICam. 

Balluff’s new industrial cameras with SWIR sensors detect object characteristics that are not visible or hard to detect for the human eye. Picture: Balluff

If you have any questions about our products, please come see us in hall 7A at booth 303. We are looking forward to seeing you there!

About Balluff 

Founded in Neuhausen auf den Fildern, Germany, in 1921, Balluff and its 3,900 employees worldwide stand for innovative technology, quality, and experience in industrial automation across various industries. As a leading sensor and automation specialist, the fourth-generation family business offers a comprehensive portfolio of high-quality sensor, identification, network, and software solutions.  

In 2023, the Balluff Group recorded sales of around 599 million euros. In addition to its headquarters in Neuhausen auf den Fildern, Balluff has sales, production and development sites around the globe and is represented by 38 subsidiaries and other agencies in 61 countries. This guarantees customers rapid worldwide availability of products and a high quality of support and service directly on site.  

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.

Contact us directly by phone: +49 7158 173-555


Balluff GmbH

Zabergäustraße 8
73765 Neuhausen a.d.F.

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue