Products
Service & Support
Industries & Solutions
Career
Company

08.12.2021

The new communication standard for intelligent factory automation

IO-Link Wireless from Balluff

The new communication standard for intelligent factory automation: IO-Link Wireless from Balluff

With its wireless IO-Link variant, Balluff is expanding its portfolio with a fast, reliable and flexible solution – while guaranteeing consistent system integration and compatibility. IO-Link Wireless is used wherever classic data transmission was previously impossible or only possible with difficulty.

As a digital interface, the IO-Link communication standard enables fieldbus-independent point-to-point connection and seamless communication between intelligent sensor and automation system. The technology is thus an essential building block for the factory of the future. With the introduction of IO-Link Wireless, Balluff is now adding a wireless solution to its own extensive IO-Link portfolio. "Whether in inaccessible places, in robotics or in highly dynamic transport systems: IO-Link Wireless promises an even more flexible and sustainable application – while maintaining system integration and compatibility," says Balluff Product Manager Michael Zahlecker. Customers already using IO-Link can easily configure IO-Link Wireless via the integrated web server.

Instead of using cables, the wireless master receives the sensor data by radio via a bridge or hub. "The new wireless standard meets the high demands of factory automation," says Zahlecker. Easier planning and installation, greater flexibility and mobility, and the elimination of plugs or cables are among the major advantages over a wired system. At the same time, IO-Link Wireless can be used worldwide without a license in a frequency range of 2.4 - 2.483 GHz. "When developing IO-Link Wireless, high reliability was of paramount importance to us," explains Zahlecker. A latency of 5ms and an error rate of 10-9 thus enable direct connection as well as fast and reliable data transmission. A further plus point is the problem-free scaling and extended integration of up to 40 devices.

The wireless IO-Link variant is used in dynamic, fixed and mobile applications: On transport systems with high speeds, compatible sensors can thus be placed directly on the carriage for more precise monitoring. When changing tools on a gripper, the absence of cabling enables data transmission in confined spaces. This also applies to milling machines, which offer little space for sensors but require high process reliability. Here, the new system scores with its robustness. "Since there is no need for cabling, IO-Link Wireless can also be used to install condition monitoring sensors in monitoring systems, even in inaccessible places," explains Zahlecker, "making the system ideally suited for retrofitting existing solutions." In addition to the new IO-Link wireless standard, Balluff offers various solutions for contactless data and power transmission and is constantly expanding its own wireless portfolio. "Using wireless technology, we want to unleash industrial communication," says Hubertus Breier, Head of Technology at Balluff, describing the benefits of wireless solutions in industrial communication. "Thanks to the IO-Link wireless standard, we can now collect data in applications, for example, where this was either technically impossible or too costly before."

About the company Balluff

The success story of Balluff began exactly 100 years ago with the set up of a precision mechanics repair workshop in Neuhausen a. d. F. On the occasion of the 100-year anniversary, with 3600 employees worldwide, the global company stands for innovative technology, quality and cross-sector experience in industrial automation. As leading sensor and automation specialist, this family-owned company in its fourth generation offers a comprehensive portfolio of high-quality sensor, identification, network and software solutions. In 2019, the Balluff Group reported revenue of around EUR 469 million. With 38 subsidiaries and other representatives in a total of 68 countries, Balluff guarantees fast worldwide availability of the products and a high caliber of advice and service locally.

Downloads

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.

Contact us directly by phone: +49 7158 173-555


Balluff GmbH

Zabergäustraße 8
73765 Neuhausen a.d.F.

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue