Products
Service & Support
Industries & Solutions
Company

How do I wire my 3-wire sensors?

All 3-wire sensors, regardless of technology (inductive, photoelectric, capacitive), are wired similarly

Shawn Day
28 Aug 2024 | 10:37 Clock

Reading Time: minutes

Three-wire sensors are used in various applications from detecting parts to locating position of the actual machine. They can come in all different technologies such as inductive sensors, photoelectric sensors and capacitive sensors, just to list a few. Although the sensor technology may differ, all 3-wire sensors are wired the same way. 

A three-wire sensor has 3 wires present: two power wires and one load wire. The power wires will connect to a power supply and the remaining wire to some type of load. The load is a device that is being controlled by the sensor. The most common type of load would be a PLC (programmable logic controller) DC input. Other examples of a load could be a relay or machine alarm. Just make sure the load rating of the sensor is not exceeded. A typical 3-wire DC sensor’s output has a rating of 100mA to 200mA.

As an example, let’s reference an inductive proximity sensor. When a target (the object that a sensor is detecting) comes within sensing range of the sensor, the sensor output turns on and current flows.

A 3-wire sensor typically is color coded with one brown wire, one blue wire and one black wire. The brown wire is the +VDC wire that connects to the positive (+) side of the power supply and the blue wire is connected to the common terminal of the power supply — this is the negative (-) terminal that is present on the power supply. The black wire is the output (load) wire of the sensor.

3-wire DC sensors can have a PNP (sourcing) or NPN (sinking) output. Just make sure the correct sensor part number is selected for the correct transistor circuit.

There you have it! As you can see wiring a 3-wire sensor is not too difficult.

Keywords

  • Basics of automation

Did you like this post?

3

Share this post

Author

Shawn Day

Shawn Day

Shawn Day has more than 25 years of manufacturing automation experience, including fifteen years at Balluff, Inc., where he serves as a technical engineer specializing in object detection related to high-speed automation, welding and stamping fabrication. He emphasizes the prevention of decreasing sensor-related machine downtime and increasing productivity. Prior to joining Balluff, Shawn worked for a Tier One automotive supplier for 15 years where he gained a vast knowledge of high-speed factory automation, with a proven record of increasing machine cycle times.


0 Contributions

Comment

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.

Contact us directly by phone: +44 1606 812777


Balluff Limited

20 Cheshire Business Park
Cheshire Avenue
Lostock Gralam
Northwich, CW9 7UA

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue