Products
Service & Support
Industries & Solutions
Company

When Color, Surface, and Transparency Become a Challenge

Why Ultrasonic Sensors Deserve a Closer Look

Jorge Castillo
29 Sep 2026 | 17:18 Clock

Reading Time: minutes

Photoelectric sensors are among the most widely used sensing technologies in industrial automation. They provide fast, reliable detection and are suitable for a broad range of applications.

However, some applications introduce challenges that can affect optical sensing performance. Changes in color, reflectivity, contamination, or transparency may require additional adjustments and can make reliable detection more difficult.

This is where ultrasonic sensors offer a different approach.

Why Some Targets Are Difficult to Detect

Photoelectric sensors rely on light to detect objects. Depending on the sensing principle and application, several target characteristics can influence detection performance.

Common challenges include:

  • Dark versus light-colored objects

  • Matte versus reflective surfaces

  • Oil, grease, or contamination on the target

  • Transparent materials such as glass or clear plastics

For maintenance teams and automation engineers, these conditions can lead to:

  • Repeated sensor adjustments

  • False triggering

  • Missed detections

  • Production interruptions


The Challenge of Transparent Materials

Transparent objects present a unique challenge because light can pass through the target rather than generating the expected signal.

Examples include:

  • Automotive windshields

  • Headlamp lenses

  • Clear plastic containers

  • Glass panels

In these applications, engineers often spend significant time optimizing sensor selection, mounting positions, reflector alignment, and background conditions to achieve reliable performance.


A Different Sensing Principle

Ultrasonic sensors operate differently.

Rather than using light, they emit sound waves and measure the time required for the echo to return from the target.

Because detection is based on sound, characteristics such as color and optical reflectivity become significantly less important.

An ultrasonic sensor can detect:

  • White or black targets

  • Matte or shiny surfaces

  • Clean or contaminated parts

  • Opaque or transparent materials

This makes ultrasonic technology especially valuable when product characteristics change during production.


Why Ultrasonic Sensors Work Well with Transparent Objects

Consider a windshield moving through an automotive assembly line.

A photoelectric sensor must successfully interact with the optical properties of the glass. Depending on the application, this may require careful system design and sensor selection.

An ultrasonic sensor approaches the challenge differently.

The question is no longer:

"Can I see the object?"

Instead, the sensor asks:

"Did my sound wave encounter an object, and how far away is it?"

This fundamentally different approach often simplifies detection in transparent-material applications.


Choosing the Right Technology

Ultrasonic sensors are not intended to replace photoelectric sensors.

Photoelectric technology remains the preferred solution for many applications requiring:

  • High-speed detection

  • Small target recognition

  • Precise positioning

  • Long sensing ranges

The real objective is selecting the sensing principle that best matches the application.

Applications involving changing colors, reflective surfaces, contamination, or transparent materials may benefit from evaluating ultrasonic technology as an alternative.


Conclusion

Successful sensor selection starts with understanding the application, not with choosing a familiar technology.

When color, reflectivity, transparency, or surface conditions create detection challenges, ultrasonic sensing provides a powerful alternative that operates independently of optical characteristics.

Sometimes the best solution is not finding a way to make a photoelectric sensor work harder.

Sometimes the better solution is to sense the target differently.

See beyond the surface. Consider ultrasonic sensing.

Keywords

  • IO-Link
  • Efficient production
  • Sensor technology
  • Robotik
  • Industrielle Automatisierung

Did you like this post?

0

Share this post

Author

Jorge Castillo

Jorge Castillo has more than 18 years of experience in industrial automation and leads Balluff’s Automotive strategy across the Americas. Having worked throughout Mexico, Argentina, Brazil, and the United States, he collaborates with OEMs, Tier 1 suppliers, and machine builders to accelerate digital transformation, improve manufacturing efficiency, and drive innovation across the automotive industry.


0 Contributions

Comment

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue