TEC Cooled vs. Uncooled SWIR Cameras
Choosing the correct SWIR camera for your application
Reading Time: minutes
When selecting a short-wave infrared (SWIR) industrial camera, one of the most important design considerations is whether to use a standard (uncooled) system or a thermoelectrically cooled (TEC) variant. Both operate in the same spectral range—typically 900 to 1700 nm—but differ significantly in performance, cost, and integration complexity due to how they manage sensor noise.
Standard SWIR Cameras
A standard SWIR camera is often the preferred choice for applications where illumination is sufficient and exposure times are short. These cameras rely on passive thermal conditions, meaning the sensor operates near ambient temperature. As a result, they are more compact, energy-efficient, and cost-effective than their cooled counterparts. This makes them ideal for high-speed inspection tasks such as food sorting, agricultural grading, or general machine vision in controlled lighting environments. Their simpler design also leads to easier system integration and improved long-term reliability, since there are fewer components that could fail.
However, uncooled SWIR sensors are more susceptible to noise—particularly dark current noise, which increases exponentially with temperature. In scenarios involving low light levels, long exposure times, or the need to detect subtle differences in material properties, this noise can significantly degrade image quality. The result may be reduced contrast, poor defect detectability, or inconsistent measurements.
TEC-Cooled SWIR Cameras
TEC-cooled SWIR cameras address this limitation by actively lowering the sensor temperature, typically by 10–30°C below ambient. This cooling dramatically reduces dark current and associated noise, enabling much higher signal-to-noise ratios. In practice, this translates to cleaner images, improved uniformity across the sensor, and greater sensitivity to fine details. Applications that benefit from this include semiconductor inspection, hyperspectral imaging, laser beam analysis, and pharmaceutical quality control—where precision and repeatability are critical.
The advantages of cooling come with trade-offs. TEC-cooled cameras are more expensive due to added components and control systems. They also consume more power and are physically larger, which can complicate integration into space-constrained systems. Additionally, thermal stabilization may introduce startup time delays, and proper heat dissipation must be considered during system design.
Below is a comparison of cooling as a method for reducing noise:
Aspect | Advantages of TEC Cooling | Disadvantages of TEC Cooling |
Noise Reduction | Significantly lowers dark current and thermal noise | Adds system complexity |
Image Quality | Higher signal-to-noise ratio and contrast | Higher upfront cost |
Sensitivity | Enables detection in low-light and long exposure scenarios | Increased power consumption |
Stability | Improved image uniformity and repeatability | Requires thermal management |
Integration | Better for high-precision applications | Larger form factor, less compact |
Operation | More consistent performance across temperatures | Potential startup stabilization time |
In summary, standard SWIR cameras are well suited for cost-sensitive, high-speed applications with adequate lighting, while TEC-cooled cameras excel in demanding environments requiring maximum sensitivity and minimal noise. The decision ultimately hinges on balancing performance requirements with system constraints such as size, cost, and power consumption.
Related topics
Keywords
- Robotik
- The basics of automation
- Trends in der Technologie
- Life Science
- Vision
- Intralogistic
- Semiconductors
Author
Alex Conradi
Alex Conradi brings nearly a decade of expertise to the automation industry, including two years of deep specialization in industrial camera technology. Throughout his career, he has focused on bridging the gap between complex hardware solutions and high-performance industrial applications.
0 Contributions