Products
Service & Support
Industries & Solutions
Company

Demo: Error proofing

Quality demands on manufacturers have been high for years, and the future will see those demands continue to rise. It is no longer good enough just to produce a high quality product. Expectations have climbed to a point where that high quality product also has to be delivered. Just-in-Time (JIT), in the proper sequence (mainly for sub components), and provide a level of traceability that enables visibility to all stakeholders.

There is no mistake - quality is an ongoing, fundamental part of any manufacturing process. It means continuous improvement. It also means that quality is everyone’s responsibility, it’s not just one department or only done at the end of the process. Error proofing devices, referred to as Poka-Yoke devices, such as sensors, need to be integrated into the process with complete traceability throughout. Also, provisions have to be in place to quickly and easily add new Poka-Yoke devices and additional traceability as requirements evolve.

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]

For Aftersales, Technical Support, Applications and
Product Inquiries we will be happy to support you: [email protected]

Feel free to contact us directly by telephone:

Inside Sales 859-727-2200 - press 1
Presales Tech Support 859-727-2200 - press 2
Aftersales Tech Support 859-727-2200 - press 3


Balluff Inc.

8125 Holton Dr.
Florence, KY 41042

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue