UHF RFID Asset Tracking in Manufacturing
How industrial environments influence RFID performance
Reading Time: minutes
UHF RFID technology enables manufacturers to automatically track and manage valuable assets such as press dies, casting molds, tooling, and workpiece carriers. When implemented correctly, UHF RFID increases asset visibility, reduces manual tracking effort, and improves operational efficiency across production and logistics processes.
However, RFID system performance depends on more than readers and tags alone. Manufacturing environments contain metal structures, harsh operating conditions, and physical constraints that can significantly influence signal quality and read reliability. Understanding these factors is essential for building a robust RFID solution that consistently delivers accurate asset data.
TL;DR
Metal surfaces can reflect, absorb, or block RFID signals, reducing read reliability.
Choosing the correct RFID tag and mounting position is critical for successful asset tracking.
High temperatures, humidity, vibration, and chemicals require industrial-grade RFID components.
Antenna placement and reader power settings have a major impact on read accuracy.
Site surveys and feasibility studies help validate RFID performance before deployment.
Why do metal surfaces create challenges for UHF RFID systems?
Metal is one of the most significant sources of RFID interference in industrial environments.
Because UHF RFID operates using radio frequencies, metal surfaces can reflect, attenuate, or completely block signals between readers and tags. The result may be reduced read ranges, inconsistent tag detection, or unintended reads from nearby assets.
This challenge is especially relevant when tracking metallic assets such as dies, molds, fixtures, and machine tooling. In these applications, RFID system design must account for the presence of metal from the very beginning. Rather than relying solely on higher reader power, successful systems combine appropriate tag technology, optimized mounting strategies, and carefully planned antenna positioning.
Proper RFID tag selection is the foundation of reliable asset tracking
How should RFID tags be selected for industrial assets?
RFID tags should be selected based on the material they will be mounted on and the environmental conditions they must withstand.
Tags designed for plastic surfaces often perform poorly when attached directly to metal. For metallic assets, manufacturers should use RFID tags specifically designed for on-metal installation or applications with defined clearance zones.
Tag size is another important consideration. Larger tags typically support longer read ranges, while compact tags may be required where installation space is limited. The optimal choice depends on the balance between available space, environmental conditions, and required reading distance. and feasibility studies
Why is mounting position important?
Even a high-performance RFID tag can fail if it is mounted incorrectly.
Tags should be positioned so they have maximum exposure to the reader antenna while remaining protected from mechanical damage. Consistent orientation across similar assets improves predictability and system reliability.
Avoid placing tags in recessed metallic cavities, directly behind obstructions, or in locations where physical wear may damage the tag. Following manufacturer-specific mounting recommendations helps maximize read performance and reduce commissioning effort.
Harsh industrial environments require rugged RFID solutions
Industrial manufacturing environments expose RFID components to conditions that are far more demanding than traditional warehouse or office applications.
Extreme heat, humidity, dust, vibration, oils, cleaning agents, and chemicals can all affect the long-term performance of RFID systems. To ensure reliable operation, both tags and antennas must be selected according to the environmental requirements of the application.
A typical example is high-temperature manufacturing. Specialized RFID tags and protective housings can tolerate temperatures of up to 220°C (428°F). However, these tags often need to cool below operational thresholds before reliable reading or writing can occur without risking damage to the tag.
When evaluating RFID hardware, manufacturers should consider:
Temperature resistance
Chemical compatibility
Protection against moisture and dust
Mechanical robustness
Expected asset lifetime
Selecting components based on environmental requirements improves uptime and reduces maintenance costs.
Antenna placement determines system performance
Why is antenna positioning critical?
RFID reader antennas must be positioned so they can reliably capture tags within the intended read zone.
Physical barriers, machinery, storage racks, and metallic structures can weaken or redirect RFID signals. Poorly positioned antennas often create dead spots where assets cannot be identified consistently.
Using multiple antennas at different locations and orientations can improve read coverage and compensate for varying asset positions. The goal is not maximum coverage but controlled coverage that supports the business process.
Successful antenna design considers:
Asset movement direction
Reading distance requirements
Potential signal reflections
Physical obstructions
Read zone boundaries
Reader power settings must balance range and accuracy
Can higher reader power improve RFID performance?
Not always.
While increasing reader power can extend read range, excessive power may also cause unintended tag reads outside the desired tracking area. In asset tracking applications, these false reads can reduce location accuracy and create confusion within maintenance, production, or inventory management systems.
The objective is to create clearly defined read zones where only relevant assets are detected.
Optimal performance is achieved by balancing:
Reader output power
Antenna placement
Tag type
Asset movement patterns
Software filtering rules
A well-configured system delivers both reliable reads and accurate location information.
Site surveys and feasibility studies reduce implementation risk
RFID projects typically achieve higher success rates when validation is performed before full deployment.
An initial site survey helps identify environmental challenges such as metal interference, physical obstructions, required read distances, and asset movement patterns. It also determines whether UHF RFID is technically suitable for the intended application.
If the concept appears viable, a more detailed feasibility study can define:
RFID tag selection
Antenna configuration
Reader locations
System topology
Physical distances and angles
Required power settings
This process minimizes implementation risks and helps ensure reliable performance once the system goes live.
Reliable RFID performance is the result of system design
Successful UHF RFID applications do not depend on a single component. Reliable asset tracking is achieved when tags, antennas, readers, software configuration, and environmental conditions are considered together as part of an integrated system design.
Takeaways
Metal surfaces remain the primary challenge in many industrial RFID applications.
The correct combination of tag selection and mounting strategy significantly improves read rates.
Industrial environments require RFID components specifically designed for harsh conditions.
Antenna placement often has a greater impact on performance than increasing reader power.
Site surveys and feasibility studies help avoid costly redesigns later.
Properly designed UHF RFID systems can improve asset visibility, productivity, and manufacturing efficiency.
FAQ
When does an industrial RFID project require a feasibility study?
A feasibility study is recommended whenever metallic structures, long reading distances, complex asset movements, or demanding environmental conditions may affect RFID performance.
Does UHF RFID replace barcode-based asset tracking?
Not necessarily. Many manufacturers use RFID and barcodes together. RFID enables automated, non-line-of-sight identification, while barcodes remain useful for manual processes and visual verification.
What is the most common cause of RFID read failures in manufacturing?
Metal interference is one of the most common causes. Reflections and signal attenuation can significantly reduce read reliability when applications are not designed specifically for metallic environments.
Can RFID be used in foundries or high-temperature production areas?
Yes. Specialized industrial RFID tags are available for high-temperature applications, although reading and writing may only be possible after the tag cools below certain operating limits.
How often should RFID system performance be reviewed?
Performance should be reviewed whenever production layouts, asset designs, material flows, or machinery configurations change, as these factors can alter signal behavior and read reliability.
Keywords
- RFID
Author
Kyle Bause
Kyle is a Product and Application Specialist at Balluff, where he works directly with manufacturers on sensor, IO-Link, and industrial connectivity applications. He spends most of his time on plant floors helping teams match technology to what their operations actually need.
0 Contributions
Comment
Popular posts
An easy way to remember PNP and NPN sensor wiring
Real-time speed of IO-Link wired
Advantages of inductive proximity sensors in industry
Automation for intralogistics: a practical perspective
Contact form
Do you have any questions or suggestions? We are at your disposal.
Balluff GmbH
-
Zabergäustraße 8
73765 Neuhausen a.d.F.