Products
Service & Support
Industries & Solutions
Company

Inductive proximity sensor targets – Material does matter

Maximizing sensor performance: how target material impacts inductive proximity sensors

Shawn Day
18 Jun 2024 | 17:02 Clock

Reading Time: minutes

From some of the previous blogs, it has been indicated that a number of variables can affect the actual sensing range achieved by an inductive proximity sensor. One of those variables mentioned was target composition or target material. Let’s review how various target materials can affect an inductive sensor’s performance.

In general the best target for an inductive proximity sensor is a flat piece of ferrous metal. Per the IEC specification the “test target” for an inductive proximity sensor is a piece of carbon steel (Fe360) that is 1 mm thick. The size of the target is square and for a standard range sensor it is typically equal to the size of the sensor’s active surface. For an M8 sensor with Sn = 1.5 mm, it would be 8 mm square; for an M12 sensor with Sn = 2 mm it would be 12 mm square, etc.

In the real world target material types can vary. As indicated above the target material that will result in the best sensing range is ferrous steel. Other non-ferrous target materials can still be detected by an inductive sensor, but normally at a reduced sensing range. To give you an idea of the amount of reduction, a chart of “correction factors” is given below.

Typical material correction factors

Material

Correction Factor

Type of Metal

Steel (Fe360)

1.0

Ferrous

Stainless Steel

0.6…1.0

Non-Ferrous

Aluminum

0.30…0.45

Non-Ferrous

Brass

0.35…0.50

Non-Ferrous

Copper

0.25…0.45

Non-Ferrous

The chart provides approximate “correction factors” as most metals are compounds rather than pure so the effective sensing range achieved will vary depending on the composition. As and example – if a standard inductive sensor had an effective sensing range of 10 mm with a ferrous steel target, that same sensor would have approximately a 3.0 mm to 4.5 mm effective sensing range with an non-ferrous aluminum target.

The main concept to keep in mind is that an inductive proximity sensor can detect a variety of ferrous and non-ferrous metals – but not necessarily at the same sensing range. Normally a non-ferrous target material will result in a shorter sensing distance.

If you need to overcome this target material sensing reduction, a number of options exist:

  1. Rather than using a standard range sensor, look for an extended range model such as a double or triple sensing range version.

  2. If the application will allow – use a non-shielded sensor rather than a shielded sensor (provides longer sensing range).

  3. Many sensors exist today that can detect ferrous and non-ferrous models at the same distance. These are sometimes known as “Universal” or “Factor 1” sensing types.

Sensor selection can be chosen to minimize the affects of varying target materials as long as the target sensing characteristics are understood in the beginning.

Keywords

  • Basics of automation

Did you like this post?

1

Share this post

Author

Shawn Day

Shawn Day

Shawn Day has more than 25 years of manufacturing automation experience, including fifteen years at Balluff, Inc., where he serves as a technical engineer specializing in object detection related to high-speed automation, welding and stamping fabrication. He emphasizes the prevention of decreasing sensor-related machine downtime and increasing productivity. Prior to joining Balluff, Shawn worked for a Tier One automotive supplier for 15 years where he gained a vast knowledge of high-speed factory automation, with a proven record of increasing machine cycle times.


6 Contributions

Comment

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]
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
In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue