Products
Service & Support
Industries & Solutions
Company

Add Automation to Gain Safety and Control in Manufacturing

Reducing risks and fostering collaboration on the shop floor

Balluff AMER
10 Dec 2024 | 22:58 Clock

Reading Time: minutes

Industry automation not only has a positive effect on the improvement of production processes, it also significantly improves employee safety. New technologies can minimize the need for employees to work in dangerous situations by replacing them all together or by working cooperatively alongside them.

Overcoming fears of automation

Many workers fear technological progress due to the generally accepted view that robots will replace people in their workplaces. But their fears are conjecture. According to a study published in 2017 by scientists at the Universities of Oxford and Yale, AI experts predict a 50% chance of AI outperforming humans at all tasks within 45 years. But, instead of replacing all workers, there is a stronger chance AI will eliminate dangerous manual labor and evolve other roles. Following are a few examples.

Automation in palletizing systems

Before automation-based solutions entered factories, laborers had to do most work by hand. A work system based on the strength of the human body, however, does not bring good results. Workers tire quickly, causing a decrease in their productivity. And with time, health problems related to regularly carrying heavy daily loads also begin to appear. Until recently, employees of the palletizing departments struggled with these problems. But today, robots are carrying out the work of moving, stacking, and transporting products on pallets.

Automation forging processes

Also, until recently, forging processes in the metallurgical industry were performed with the help of human workers. There are still factories today in which blacksmiths are responsible for putting the hot metal element under the hammer to form the final shape of the product. Such a device hits with a force of several dozen tons, several times a minute. Being at the hammer is therefore extremely dangerous and may cause permanent damage to the worker’s health. Elevated temperatures in the workplace can also have negative effects on the body.

At most businesses, forging processes are now fully automated. Robots specially prepared for such work feed the elements to the automatic hammer with their grippers. And sensory solutions help make the job safer by detecting the presence of people or undesirable elements within the working machine. The quality control of manufactured products is also extremely important and more easily controlled with an automated system.

Automation in welding processes

Welding processes are another dangerous activity in which automation is starting to play a key role. During welding work, toxic fumes are released from the gas lagging, which the welder regularly inhales. This can result in serious poisoning or chronic respiratory diseases. Welding also produces sparks which can lead to severe burns and worker blindness.

Again, automation makes the process safer. High-class welding machines exist on the market that can work continuously, under human control. With such solutions, it is necessary to use appropriate protection systems to protect employees against possible contact with machines during work. Automation in this situation eliminates a dangerous role, and creates a new, safer, and, some would say, better work role.

Skillful design of automation systems

While factory automation eliminates some threats to workers, others often arise, creating the need for strict design plans prepared by specialists in this field. It is necessary to prepare the automation system in such a way that it not only ensures safety, it does so without reducing productivity or creating downtime which can cause the employee to bypass security systems. The systems blocking the working space of the machine should not interfere with the worker and the worker should not interfere with the system. Where possible, instead of a mechanical lock, an optical curtain at the feeding point should be used to stop the machine’s operation if a foreign object breaks the curtain’s beam of the light. Mechanical locks blocking access to the working space should be in places where it is not necessary to open the door frequently.

Successful human-machine collaboration

When designing automation systems in production companies, it is also necessary to remember that often a human is working alongside the robot. In palletizing systems, for example, a person is responsible for preparing the place for packing and cleaning the working area. For the work to go smoothly, it may be worth creating two positions next to each other. Mechanisms on the market today allow you to control the work of robots at a given position, assigning them to the workspace. Special security scanners prevent the robots from moving to positions where someone is working.

Keywords

  • Basics of automation

Did you like this post?

0

Share this post

Author

Balluff AMER


25 Contributions

Comment

Discover related topics

More from the author

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]
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
In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue