Products
Service & Support
Industries & Solutions
Company

How to understand the difference between resolution, accuracy, and repeatability / precision

Measurement performance: differentiating resolution, accuracy, and repeatability

Jack Moermond
25 Jun 2024 | 22:04 Clock

Reading Time: minutes

Scott’s article on analog resolution provides a great explanation of analog signal resolution and how to calculate an analog sensor's resolution. The blog post expands on that one with a brief summary of typical performance criteria -- resolution, accuracy, and repeatability -- of linear measurement systems.

Resolution

The output resolution of your sensing device determines the smallest possible physical change your device is able to detect. One has to distinguish here between theoretical and practical resolution. In theory, a given linear motion sensor might give you 4 nm resolution, but practically, your motion system will never be able to make 4 nm steps due to mechanical compliance, friction and mechanical backlash.

Low resolution

High resolution

Accuracy

Accuracy describes for a specific point the difference between the actual position of your drive system and the position as measured by the measurement device. The actual achievable system accuracy depends on all components of the system including mechanical tolerances and backlash, and load weight, as well as programming algorithms.

Low accuracy, low repeatability

Repeatability

Repeatability is defined as the range of actual positions the system takes while being repeatedly commanded to the same location under identical conditions. Some linear measurement systems differentiate between unidirectional and bidirectional repeatability, which defines if the target has been approached from only one direction or from both.

A comparison between the two provides additional information about backlash and hysteresis of the measurement device. Most manufacturers of servo and encoder systems specify repeatability as +/- resolution, which of course doesn’t factor in any remaining parts of the motion system.

Low accuracy, high repeatability

Precision

Precision is a synonym for repeatability, described above.

High accuracy, high repeatability

The most difficult part in the specification of a motion or measurement feedback system is finding the right balance between all of the components involved to achieve the desired system performance at the best cost level. A highly accurate and repeatable measurement device alone cannot compensate for low mechanical system compliance or ineffective program logic and vice versa.

Keywords

  • Basics of automation

Did you like this post?

0

Share this post

Author

Jack Moermond

Jack Moermond


6 Contributions

Comment

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]
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
In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue