Products
Service & Support
Industries & Solutions
Company

Control Meets IIoT, Providing Insights into a New World

Learn to leverage external systems for condition monitoring and enhanced control

Mark Sippel
10 Dec 2024 | 21:53 Clock

Reading Time: minutes

In manufacturing and automation control, the programmable logic controller (PLC) is an essential tool. And since the PLC is integrated into the machine already, it’s understandable that you might see the PLC as all that you need to do anything in automation on the manufacturing floor.

Condition monitoring in machine automation

For example, process or condition monitoring is emerging as an essential automation feature that can help ensure that machines are running smoothly. This can be done by monitoring motor or mechanical vibration, temperature or pressure. You can also add functionality for a machine or line configuration or setup by adding sensors to verify fixture locations for machine configuration at changeovers.

One way to do this is to wire these sensors to the PLC, modify its code, and use it as an all-in-one device. After all, it’s on the machine already. But there’s a definite downside to using a PLC this way. Its processing power is limited, and there are limits to the number of additional processes and functions it can run. Why risk possible complications that could impact the reliability of your control systems? There are alternatives.

External monitoring and support processes

Consider using more flexible platforms, such as an edge gateway, Linux, and IO-Link. These external sources open a whole new world of alternatives that provide better reliability and more options for today and the future. It also makes it easier to access and integrate condition monitoring and configuration data into enterprise IT/OT (information technology/operational technology) systems, which PLCs are not well suited to interface with if they can be integrated at all.

Here are some practical examples of this type of augmented or add-on/retrofit functionality:

  • Motor or pump vibration condition monitoring

  • Support-process-related pressure, vibration and temperature monitoring

  • Monitoring of product or process flow

  • Portable battery-based/cloud condition monitoring

  • Mold and Die cloud-based cycle/usage monitoring

  • Product changeover, operator guidance system

  • Automatic inventory monitoring warehouse system

Using external systems for these additional functions means you can readily take advantage of the ever-widening availability of more powerful computing systems and the simple connectivity and networking of smart sensors and transducers. Augmenting and improving your control systems with external monitoring and support processes is one of the notable benefits of employing Industrial Internet of Things (IIoT) and Industry 4.0 tools.

The ease of with which you can integrate these systems into IT/OT systems, even including cloud-based access, can dramatically change what is now available for process information-gathering and monitoring and augment processes without touching or effecting the rudimentary control system of new or existing machines or lines. In many cases, external systems can even be added at lower price points than PLC modification, which means they can be more easily justified for their ROI and functionality.

Keywords

  • Condition monitoring
  • IO-Link

Did you like this post?

0

Share this post

Author

Mark Sippel

Mark Sippel

Mark Sippel is the Manager fort he TAS (Technical Applications and Solutions engineering team fort he United States. The TAS team helps customers develop application solutions and determine the best Balluff products for that solution.


21 Contributions

Comment

Discover related topics

More from the author

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]

For Aftersales, Technical Support, Applications and
Product Inquiries we will be happy to support you: [email protected]

Feel free to contact us directly by telephone:

Inside Sales 859-727-2200 - press 1
Presales Tech Support 859-727-2200 - press 2
Aftersales Tech Support 859-727-2200 - press 3


Balluff Inc.

8125 Holton Dr.
Florence, KY 41042

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue