Be Driven by Data and Decrease Downtime
Turn real-time machine data into actionable insights that boost quality and keep production running smoothly
Reading Time: minutes
Being “driven by data” is simply the act of making decisions based on real data instead of guessing or basing them on theoretical outcomes. Why one should do that, especially in manufacturing operations, is obvious. How it is done is not always so clear.
Here is how you can use a sensor, indicator light, and RFID to provide feedback that drives overall quality and efficiency.
Machine Condition Monitoring
You’ve heard the saying, “if it ain’t broke, don’t fix it.” However, broken machines cause downtime. What if there was a way to know when a machine is getting ready to fail, and you could fix it before it caused downtime? You can do that now!
The two main types of data measured in manufacturing applications are temperature and vibration. A sudden or gradual increase in either of these is typically an indicator that something is going wrong. Just having access to that data won’t stop the machine from failing, though. Combined with an indicator light and RFID, the sensor can provide real-time feedback to the operator, and the event can be documented on the RFID tag. The machine can then be adjusted or repaired during a planned maintenance period.
Managing Quality
A machine on its way to failure can produce parts that don’t meet quality standards. Fixing the problem before it affects production prevents scrap and rework and ensures the customer is getting a product with the quality they expect.
Managing Efficiency
Unplanned downtime costs thousands of dollars per minute in some industries. The time and resources required to deal with a failed machine far exceed the cost of the entire system designed to produce an early warning, provide indication, and document the event.
Quality and efficiency are the difference makers in manufacturing. That is, whoever makes the highest quality products most efficiently usually has the most profitable and sustainable business. Again, why is obvious, but how is the challenge. Hopefully, you can use the above data to make higher quality products more efficiently.
Keywords
- Condition monitoring
Author
Balluff AMER
25 Contributions