Products
Service & Support
Industries & Solutions
Company

IO-Link Benefits in Robotic Weld Cell Tooling

Simplifying cabling, expanding flexibility, and reducing costs

Balluff AMER
11 Dec 2024 | 18:36 Clock

Reading Time: minutes

Working previously as a controls engineering manager in robotic welding, I have seen some consistent challenges when designing robotic weld cell systems.

For example, the pre-engineered-style welding cells I’ve worked with use many types of tooling. However, space for tooling and cabling is limited, and so is the automation on board. Some use a PLC function, and others use a robot controller to process data.

One approach that worked well was to use IO-Link in the systems I designed. Its simple open fieldbus communication interface and digital transmission brought a number of benefits.

  1.  IO-Link’s digital signals aren’t affected by noise, so I could use smart sensors and connect them with unshielded 4-pin cables.

  2.  Expandability was easy, either from the Master block or by adding discrete I/O modules.

  3.  IO-Link can use the block's ID to identify the fixture it is associated with and ensure the correct fixture is in the correct location.

  4.  Cabling is simplified with IO-Link since the IO-Link Master can control inputs, outputs, and valve packs. The only cables needed will be 24V power, Ethernet, weld ground (depending on the system), and air.

  5.  Fewer cables mean less cost for cables and installation, improved cable management, and fewer cables to run through a tailstock or turntable access hole.

One system I designed used one IO-Link Master block, three discrete I/O modules, and one SMC valve manifold controlled via IO-Link. This tooling had 16 clamps and 10 sensors, requiring 42 total inputs and controlling 16 valves. The system worked very well with this setup!

Another note: It’s good to think beyond the process at hand to how it might be used in the future. A system built on IO-Link is much more adaptable to different tooling when a change-over is needed. Click here to read more about how to use IO-Link in welding environments.

Keywords

  • Robotics

Did you like this post?

0

Share this post

Author

Balluff AMER


25 Contributions

Comment

Discover related topics

More from the author

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]
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
In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue