Products
Service & Support
Industries & Solutions
Career
Company

Intralogistics in Metalworking

Boosting Efficiency

21 Feb 2024 | 16:40 Clock

Reading Time: minutes

Due to the shortage of skilled workers, manufacturing companies in metalworking are automating their production processes more and more. The goals here are, for example, to increase the output rate and at the same time to be able to react flexibly to changing customer requirements.

In order to improve the utilization and overall equipment effectiveness of machine tools, the production engineers plan automation solutions for the automatic loading and unloading of workpieces. For both CNC machining centers and for CNC lathes. Machine tool builders offer appropriate automation equipment as an option with the sales of new machines.

Automated feeding of workpieces

Individual robots typically are assigned to one machine, They offer flexibility for small to medium-sized production batches. Robots are available in different types (articulated robot mostly used in this application) and sizes (depending on the weight of the workpiece).

In manufacturing of large series parts, e.g. in the automotive industry, gantry robots often transport the workpieces. From one machining center to the next. This has the advantage that standard machines do the machining. Production engineers optimize the cycle times and cycle rates for the workpieces. They do this by dividing the individual machining steps (rough machining, pre-drilling, finishing, finish drilling, …) on several machines.

Bin picking

Raw parts in series production are often stored as bulk goods in lattice boxes. Robots or so-called Cobots remove the workpieces from the lattice box and feed them to the processing machine. 3D cameras provide information for correct gripping of the object to the robot control system.

Identification of objects for lot size 1

To achieve a highly flexible production of individual parts, the machine control needs to know which workpiece will be processed in the next step.

Optical codes like barcode or datamatrix codes offer the possibilities of serialization as a basic condition for the setup of a smart factory

For a long time, RFID has been established for the identification of cutting tools in milling centers. The RFID data carrier is located in the tool holder (steep taper SK, hollow shank taper HSK, …) or in the pull stud.

RFID now finds its way to the application field of workpiece tracking.

This way, RFID combines the use of tool identification and tracking workpieces in production. RFID processor units with multiple interfaces to connect several RFID read/write heads realize an economical communication to the machine control system.

The current activities to standardize interfaces in the area of ​​location technologies for intralogistics will open up additional application fields for RFID.

Conclusion

The core technologies of machine tools (such as CNC machine control, optimization of cutting processes) have made tremendous progress in metalworking in the last few decades. Now the focus is on the periphery, on optimizing the logistical processes for workpiece handling.

Keywords

  • IO-Link
  • Innovations

Did you like this post?

0

Share this post

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.

Contact us directly by phone: +49 7158 173-555


Balluff GmbH

Zabergäustraße 8
73765 Neuhausen a.d.F.

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue