Products
Service & Support
Industries & Solutions
Career
Company

On the way to intelligent hydraulics with IIoT connection

From hydraulic system to digital drive solution

Balluff EMEA
24 Apr 2024 | 15:57 Clock
Application example from hydraulic system to digital drive solution

Reading Time: minutes

About a decade ago, the world was first confronted with the concept of Industry 4.0 at the Hannover Messe trade fair. A year later, General Electric coined the term 'Industrial Internet'. Back then, these ideas were still visions. Today, we are witnessing an industrial revolution in which intelligent, digitally networked hydraulic solutions are also becoming a reality.

Industry 4.0 marks the fourth phase of the industrial revolution, characterized by the integration of cyber-physical systems into machines and plants. The previous phases included mechanization in the late 18th century, the introduction of the division of labour and new energy sources in the late 19th century and automation, which began in the late 1960s with the development of programmable logic controllers (PLCs).

The Industrial Internet of Things (IIoT) is the catalyst that makes Industry 4.0 possible. It allows the integration of advanced sensors, digitized drives and other field devices to make processes more efficient. In fluid technology, for example, smart sensors are used to monitor various parameters in hydraulic systems such as temperature, pressure, flow, fill level and the stroke and position of actuators. These sensors provide real-time information about hydraulic processes and components that can be analysed and visualized to improve processes.

(1) Machine control (2) Analysis, data documentation in the cloud (3) Monitoring, Visualization of the recorded data (4) Autonomous axis in the field level (5) Recording the flow of fluid media with thermal flow monitors BFF (6) Temperature measurement with temperature sensors BFT (7) Valve parameterization via IO-Link (8) Pressure measurement with pressure sensors BSP (9) Continuous level detection with magnetostrictive position measuring systems BTL (10) Level control via level detection with capacitive sensors BCS

This is also facilitated, for example, by the IO-Link communication standard, which enables parameterization and communication from the field level via the control system to the cloud.

Today, intelligent hydraulics are used in a wide range of industries, processes and applications, from the iron and steel industry to stamping in the automotive sector and wind farms.

It remains exciting to see what innovations the next ten years will bring ...

Keywords

  • Industrial Networking
  • IO-Link

Did you like this post?

0

Share this post

Author

Balluff EMEA

Balluff EMEA

We are your partner for innovative solutions in industrial automation. With our passion we improve your competitive position with speed and results. With our 100 years company history and more than 60 years of sensor experience, Balluff is a world leader and one of the most efficient manufacturers of sensor technology.


45 Contributions
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
For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.

Contact us directly by phone: +49 7158 173-555


Balluff GmbH

Zabergäustraße 8
73765 Neuhausen a.d.F.

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue