Products
Service & Support
Industries & Solutions
Company

Understanding the significance and color codes of stack lights in industrial machinery

Stack lights offer efficient communication, warnings, enhanced safety, and customizable color codes for specific uses

John Takacs
04 Apr 2024 | 22:19 Clock

Reading Time: minutes

Stack lights, also known as signal towers or smart lights, are commonly used in industrial settings to visually convey machinery or process status. These lights consist of a vertical stack of colored lights that are easily seen from a distance. The importance in industrial machinery lies in providing quick and clear visual indicators, improving workplace communication and safety.

Key functions advantages

Stack lights in industrial settings offer the following key advantages:

Status indication: Operators and workers often use stack lights to indicate the operational status of a machine or process. See below the different colors representing different conditions, allowing for quick assessments of situations. Operators and workers often use stack lights to indicate the operational status of a machine or process.

Warning and alert signals: Stack lights can be configured to emit specific colors, warning of potential issues or alerting personnel to take specific actions. For example, a flashing red light might indicate a critical fault or emergency.

Efficient communication: The use of colors in stack lights provides an efficient and intuitive means of communication. Even in noisy or busy industrial environments, workers can easily understand the status or conditions indicated by the lights.

Increased safety: By providing immediate visual feedback, stack lights contribute to a safer working environment. Operators can respond promptly to changes in machine status or emergency situations, reducing the risk of accidents.

Customization: You can customize stack lights to suit specific applications by configuring the sequence of colors, determining the meaning of each color, and designing the overall layout to match the needs of the facility.

Decoding stack light color codes

Specific color codes can vary between industries and applications, so it is essential to refer to the documentation provided by the equipment manufacturer or follow industry standards for consistent use. The following are some common color codes:

Green typically indicates that the machine or process is in normal operation or that a specific condition is met.

Yellow/amber is often a warning signal, indicating a cautionary state or a need for attention without immediate danger.

Red indicates a critical or emergency condition requiring immediate attention. It can signal a fault, shutdown, or other urgent issues.

Blue sometimes displays a maintenance or service in progress. It can also represent a specific machine status depending on the system configuration.

White conveys a particular status, such as a change in production mode, or it can have a custom meaning based on the application.

In summary, stack lights are essential in conveying machinery or process status in industrial settings. Their advantages include efficient communication, warning signals, increased safety, and customization for specific applications through color codes.

Keywords

  • Basics of automation

Did you like this post?

2

Share this post

Author

John Takacs

John Takacs

Global Key Account Manager Automotive OEM, 25+ years of Automation Sales, Account Management and large project management with Machine builders and Automotive Manufacturing


12 Contributions

Comment

Discover related topics

More from the author

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]
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
In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue