Weighing the Pros and Cons for Optimal Performance: Standard vs. Customized Sensors
Choosing between standard and customized sensors for specific applications.
Reading Time: minutes
Sensors are crucial for monitoring environments, gathering data, and facilitating automation. Several off-the-shelf solutions from a variety of reputable suppliers exist to satisfy the sensor needs of most industrial assembly lines. But when it comes to selecting sensors to perform a specific task, such as a medical device, lab automation equipment, or semiconductor tools, the choice often comes down to a standard industrial sensor or a customized solution. Each option has its advantages and disadvantages, and understanding these can help design engineers make informed decisions based on their unique requirements.
Pros of customized sensors
1. Tailored functionality: The most significant advantage of customized sensors is their ability to be tailored to meet specific application needs. Customization ensures that sensor parameters such as sensitivity, range, response time, and form factor precisely match the requirements of the intended application. This level of customization typically results in enhanced performance, a more streamlined fit, and improved integration into the customer’s device.
2. Optimized cost-efficiency: Customization typically comes with upfront costs for developing a sensor for a specific purpose, but it can lead to long-term cost savings. By eliminating unnecessary features within a standard sensor and focusing on essential functionalities, customized sensors can be more cost-effective in the long run. This is especially true for high-volume production or specialized applications where standard sensors would be overkill.
3. Improved integration: Customized sensors can be designed to integrate into devices cleanly, eliminating the need for additional brackets or modifications to fit a universal sensor. This integration capability simplifies installation, reduces labor time, and creates a more robust solution, reducing downtime caused by misadjusted sensors.
4. Enhanced performance: By leveraging advanced technologies and materials, customized sensors can deliver superior performance compared to standard sensors. They can achieve higher accuracy, better resolution, and increased reliability. Custom solutions commonly start with a known technology adopted from the standard sensor. The custom sensor can then incorporate lessons learned from producing the standard sensor, using that added knowledge to push the boundaries of what is possible, enabling innovations and driving competitive advantages.
Cons of customized sensors
1. Higher development time: One primary drawback of customized sensors is the time and resources required for development and testing. Designing a sensor from scratch or modifying existing designs to meet specific requirements can be a time-consuming process, delaying deployment and potentially impacting time to market. Establishing a clear timeline with expectations and design milestones is essential for success.
2. Increased development costs: Customization often comes at a premium, with development costs including research, design, prototyping, and validation. For businesses operating on tight budgets or with limited resources, the higher upfront costs of customized sensors may present a barrier to adoption, especially when viable off-the-shelf alternatives are available.
3. Limited scalability: Customized sensors are typically optimized for specific applications, limiting their scalability across different projects or industries. Unlike standard sensors that are mass-produced and widely available, custom solutions may lack the flexibility to adapt to evolving needs or accommodate diverse applications without a redesign.
4. Dependency on expertise: Developing customized sensors requires expertise and resources, such as skilled engineers, test labs, and manufacturing facilities. For organizations lacking these in-house capabilities, outsourcing sensor development to third-party providers can introduce additional complexities, including intellectual property concerns and communication challenges.
The decision to use customized sensors vs standard sensors depends on various factors, including the specific application requirements, budget constraints, time considerations, and strategic objectives. Choosing a reputable manufacturer with a mastery of numerous sensing technologies and a proven track record of performance ensures a successful product launch. While customized sensors offer unparalleled flexibility, performance, and integration capabilities, they also entail higher development costs, longer lead times, and potential scalability challenges. Standard sensors can be cost-effective. and readily available, but may lack certain desired parameters, such as accuracy, speed, or form factor. Ultimately, original equipment manufacturers must carefully weigh the pros and cons to determine the most suitable sensor solution that aligns with their goals and objectives.
Keywords
- Industrial automation
Author
Robert Crumley
Rob Crumley is the Industry Account Manager – Semicon at Balluff, Inc. He brings 12 years of engineering experience across manufacturing, controls, and applications roles, along with 24 years in sales, including key account management and business development responsibilities. His expertise in sensing technologies helps customers solve complex automation and semiconductor manufacturing challenges.
23 Contributions