Products
Service & Support
Industries & Solutions
Company

Add smart condition monitoring sensors to your PLC control systems to deliver data in real time

Smart condition monitoring sensors with IO-Link offer real-time access to variables and alarms on the PLC system

Randy Dang
11 Mar 2024 | 14:29 Clock

Reading Time: minutes

Condition monitoring of critical components on machines delivers enormous benefits to productivity in a plant. Rather than have a motor, pump, or compressor unexpectedly fail and the machine be inoperable until a replacement part is installed, condition monitoring of those critical pieces on the machine can provide warning signs that something is about to go terribly wrong. Vibration measurements on rotating equipment can detect when there is an imbalance or degradation of rolling bearing elements. Temperature measurements can detect when a component is overheated and should be cooled down. Other environmental detections, such as humidity and ambient pressure, can alert someone to investigate why humidity or pressure is building up on a component or in an area.

These measurement points are normally taken by specific accelerometers, temperature probes, humidity and pressure sensors and then analyzed through high end instruments with special analysis software. Typically, these instruments and software are separate from the PLC controls system. This means that even when the data indicates a future potential issue, steps need to be taken separately to stop the machine from running.

Using smart condition monitoring sensors with IO-Link allows these measured variables and alarms to be available directly onto the PLC system in real time. Some condition monitoring sensors now even have microprocessors onboard that immediately analyze the measured variables. The sensor can be configured for the measurement limit thresholds of the device it’s monitoring so that the sensor can issue a warning or alarm through the IO-Link communications channel to the PLC once those thresholds have been hit. That way, when a warning condition presents itself, the PLC can react immediately to it, whether that means sending an alert on a HMI, or stopping the machine from running altogether until the alarmed component is fixed or replaced.

Having the condition monitoring sensor on IO-Link has many advantages. As an IEC61131-9 standard, IO-Link is an open standard and not proprietary to any manufacturer. The protocol itself is on the sensor/actuator level and fieldbus independent. IO-Link allows the condition monitoring sensor to connect to Ethernet/IP, Profinet & Profibus, CC-Link & CC-Link IE Field, EtherCAT and TCP/IP networks regardless of PLC. Using an IO-Link master gateway, multiple smart condition monitoring sensors and other IO-Link devices can be connected to the controls network as a single node.

The picture above shows two condition monitoring sensors connected to a single address on the fieldbus network. In this example, a single gateway allows up to eight IO-Link condition monitoring sensors to be connected.

Through IO-Link, the PLC’s standard acyclic channel can be used to setup the parameters of the measured alarm conditions to match the specific device the sensor is monitoring. The PLC’s standard cyclic communications can then be used to monitor the alarm status bits from the condition monitoring sensor.  When an alarm threshold gets hit, the alarm status bit goes high and the PLC can then react in real time to control the machine. This relieves the burden of analyzing the sensor’s condition monitoring data from the PLC as the sensor is doing the work.

Keywords

  • IO-Link
  • Condition monitoring

Did you like this post?

1

Share this post

Author

Randy Dang

Randy Dang

Randy Dang is an Application & Product Specialist at Balluff with more than 20 years of experience in industrial automation. For the past 13 years, he has helped customers solve sensing and automation challenges by turning complex technical requirements into practical solutions.


12 Contributions

Comment

Discover related topics

More from the author

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]

For Aftersales, Technical Support, Applications and
Product Inquiries we will be happy to support you: [email protected]

Feel free to contact us directly by telephone:

Inside Sales 859-727-2200 - press 1
Presales Tech Support 859-727-2200 - press 2
Aftersales Tech Support 859-727-2200 - press 3


Balluff Inc.

8125 Holton Dr.
Florence, KY 41042

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue