Products
Service & Support
Industries & Solutions
Company

How Edge Gateways Support Real-Time Condition Monitoring Data

Choosing the right IoT Edge Gateway for seamless data integration and communication

Randy Dang
09 Dec 2024 | 23:00 Clock

Reading Time: minutes

In my previous blog post from early summer, I talked about IO-Link sensors with condition monitoring features that work with PLCs. I covered how condition monitoring variables can be set up as alarms and how simple logic can be set up inside the sensor so it only sets off those alarms to the PLC in real time to alert operators when something is wrong. Many companies, however, take advantage of the IoT sensor data with the long-term goal of analyzing the environmental data conditions to predict maintenance needs in real time versus relying on a schedule. Some even want to connect directly to their MES systems to inform maintenance personnel of daily maintenance orders, which requires a separate device, such as an IoT edge gateway.

Edge gateway benefits

The biggest benefit of an IoT edge gateway is the ability to process and store large amounts of data quickly, enabling real-time applications to use that data efficiently.

An IoT edge gateway typically sits at the end or edge of your network and gathers all the sensor data either directly from the sensors or from the PLC. Since there will be a large amount of data from all the sensors on the network, part of the edge gateway setup is to filter the relevant and important information and process this vast amount of data. The edge gateway must also handle the amount of data required reliably, and it must have low latency. These important factors are often associated with the gateway’s CPU and memory specifications.

After looking at the performance of the edge gateway, comes the ‘gateway’ aspect which provides a translation to different communications networks, whether local or cloud-based. There are the hardware specs of the gateway, whether it’s using serial, USB or Ethernet for that connection, as well as the environmental ratings on the gateway. Then, more importantly, is the software side of the edge gateway. There are cloud-based communications standards designed for different applications and for either private or public cloud networks.

Edge gateways support different communications protocols, such as HTTPS, MQTT, RESTful API, C/Python API. The gateway portion also helps in the conversion of those protocols and the ease of interoperability to different platforms, such as AWS, Azure, Ignition, and Wonderware. This provides data transparency so that all the data gathered can be used across the many different software platforms.

To get to the IoT end goal, an edge gateway is necessary and it’s important to choose the correct one.

Keywords

  • Condition monitoring

Did you like this post?

0

Share this post

Author

Randy Dang

Randy Dang

Randy Dang is an Application & Product Specialist at Balluff with more than 20 years of experience in industrial automation. For the past 13 years, he has helped customers solve sensing and automation challenges by turning complex technical requirements into practical solutions.


12 Contributions

Comment

Discover related topics

More from the author

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]

For Aftersales, Technical Support, Applications and
Product Inquiries we will be happy to support you: [email protected]

Feel free to contact us directly by telephone:

Inside Sales 859-727-2200 - press 1
Presales Tech Support 859-727-2200 - press 2
Aftersales Tech Support 859-727-2200 - press 3


Balluff Inc.

8125 Holton Dr.
Florence, KY 41042

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue