Selecting the Right Edge Gateway for IIoT Deployment
Evaluating different edge gateways based on your specific needs will significantly impact the efficiency, reliability, and security of your IIoT deployment.
Reading Time: minutes
In my previous blog post, MQTT Protocol for Smarter Automation, I discussed how the MQTT protocol and an edge gateway can serve as a message broker, routing data from smart IoT devices to the appropriate destinations. Because MQTT brokers enable real-time communications between sensors, controllers and production systems, choosing the right edge gateway is critical for successful IIoT deployment. When selecting an edge gateway, consider factors such as compatibility, scalability, security, and ease of integration.
Understanding the role of an edge gateway
Think of an edge gateway as middleware between hardware and software. Make sure it can communicate with all factory-floor hardware devices, such as sensors and controllers, and is compatible with all various software systems. The edge gateway functions as the central hub, managing the flow of messages between the hardware devices and different software applications, eliminating the need for direct connections between hardware devices.
Because there are no direct connections between the hardware and software, the edge gateway must handle the multiple simultaneous connections and the current load of messages from devices. Its ability to manage the connections and messages is crucial for the MQTT protocol to scale effectively. Check the number of connection points available. The edge gateway can limit the load by parsing data messages, ensuring only the required data is sent to the clients.
Importance of security and integration
Security is crucial when sending sensitive data over MQTT. Two forms of security that edge gateways can provide are encryption and authentication. This typically happens via the transport layer security protocol (TLS) of the message packets. Encryption ensures that the data transmitted between clients and servers is encrypted to prevent unauthorized users from reading it. A signed certificate key decodes the encryption. The authentication verifies the identity of a client or server before allowing an established connection to the network. This can be password-based with a username and login credentials.
Lastly, consider the ease of setup, configuration, and management of devices on the hardware side. On the software side, ensure seamless integration with other communications protocols and cloud platforms. Choose edge gateways with user-friendly interfaces and comprehensive resources, such as examples and documentation for common platforms and programming languages.
Testing multiple edge gateways in a controlled environment can help you assess all their features. Considering these factors and evaluating different edge gateways based on your specific needs will significantly impact the efficiency, reliability, and security of your IoT deployment.
Keywords
- Message Queue Telemetry Transport (MQTT)
Author
Randy Dang
Randy Dang is an Application & Product Specialist at Balluff with more than 20 years of experience in industrial automation. For the past 13 years, he has helped customers solve sensing and automation challenges by turning complex technical requirements into practical solutions.
12 Contributions