Products
Service & Support
Industries & Solutions
Company

Using MQTT Protocol for Smarter Automation

Edge gateway enables MQTT devices to communicate, offering simple data collection over Ethernet

Randy Dang
11 Jun 2024 | 21:09 Clock

Reading Time: minutes

In my previous blog post, “Edge Gateways to Support Real-Time Condition Monitoring Data,” I talked about the importance of using an edge gateway to gather the IoT data from sensors in parallel with a PLC. This was because of the large data load and the need to avoid interfering with the existing machine communications. In this post, I want to delve deeper into the topic and explain the process of implementing an edge gateway.

Using the existing Ethernet infrastructure

One way to collect IoT data with an edge gateway is to use the existing Ethernet infrastructure. With most devices already communicating on an industrial Ethernet protocol, an edge gateway can gather the data on the same physical Ethernet port but at a separate software-defined number associated with a network protocol communication.

Message Queue Telemetry Transport (MQTT)

One of the most commonly used IoT protocols is Message Queue Telemetry Transport (MQTT). It is an ISO standard and has a dedicated software Ethernet port of 1883 and 8883 for secure encrypted communications. One reason for its popularity is that it is designed to be lightweight and efficient. Lightweight means that the protocol requires a minimum coding and it uses low-bandwidth connections.

Brokers and clients

The MQTT protocol defines two entities: a broker and a client. The edge gateway typically serves as a message broker that receives client messages and routes them to the appropriate destination clients. A client is any device that runs an MQTT library and connects to an MQTT broker.

MQTT works on a publisher and subscriber model. Smart IoT devices are set up to be publishers, where they publish different condition data as topics to an edge gateway. Other clients, such as PCs and data centers, can be set up as subscribers. The edge gateway, serving as a broker, receives all the published data and forwards it only to the subscribers interested in that topic.

One client can publish many different topics and subscribe to other topics, and many clients can subscribe to the same topic, making the architecture flexible and scalable.

The edge gateway serving as the broker allows devices to communicate with each other if the device supports the MQTT protocol. MQTT can connect a wide range of devices, from sensors to actuators on machines to mobile devices and cloud servers. While MQTT isn’t the only way to gather data, it offers a simple and reliable way for customers to start gathering that data with their existing Ethernet infrastructures.

Keywords

  • Message Queue Telemetry Transport (MQTT)

Did you like this post?

0

Share this post

Author

Randy Dang

Randy Dang

Randy Dang is an Application & Product Specialist at Balluff with more than 20 years of experience in industrial automation. For the past 13 years, he has helped customers solve sensing and automation challenges by turning complex technical requirements into practical solutions.


12 Contributions

Comment

Discover related topics

More from the author

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]

For Aftersales, Technical Support, Applications and
Product Inquiries we will be happy to support you: [email protected]

Feel free to contact us directly by telephone:

Inside Sales 859-727-2200 - press 1
Presales Tech Support 859-727-2200 - press 2
Aftersales Tech Support 859-727-2200 - press 3


Balluff Inc.

8125 Holton Dr.
Florence, KY 41042

Free sample product

In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue