Condition Monitoring in Packaging Machines
How OEMs improve OEE and reduce unplanned downtime
Reading Time: minutes
Packaging lines depend on fast, synchronized machines. Condition monitoring gives OEMs continuous insight into machine health, helps reveal abnormal behavior early, and supports maintenance based on actual operating condition rather than guesswork.
Why does downtime have such a large impact on packaging machines?
Downtime in packaging is a line-performance problem, not only a maintenance event. Form-fill-seal, filling, labeling, cartoning, and end-of-line systems operate as connected processes. A failure at one critical point can interrupt product flow, reduce availability, create quality losses, and lower overall equipment effectiveness (OEE).
The financial exposure can also be substantial. A 2024 survey reported by MaintainX placed the average cost of one hour of unplanned downtime at about $25,000, with costs exceeding $500,000 for larger organizations. The survey covered 1,165 maintenance, repair, and operations professionals across several sectors, so the figures should be treated as cross-industry context rather than a packaging-specific benchmark.
For OEMs, unreliable operation can increase service demand, complicate troubleshooting, and weaken confidence in the delivered machine. Designing for machine-health visibility therefore supports both the end user’s production goals and the OEM’s lifecycle-service model. In packaging applications, it can also help maintain changeover performance, process stability, and machine availability in high-speed production environments.
Why are reactive and calendar-based maintenance not enough?
Reactive maintenance waits for a failure. Preventive maintenance services equipment at fixed time or usage intervals. Both approaches remain useful in the right context, but neither consistently reflects the actual condition of every component.
ARC Advisory Group cites NASA and U.S. Navy failure-pattern data showing that 18% of failures are age- or usage-related, while 82% follow random patterns. This finding does not make preventive maintenance obsolete. It shows why fixed schedules alone can miss developing faults or trigger work on components that are still operating normally.
Maintenance strategies at a glance
Strategy | When action occurs | Best fit | Main limitation |
Reactive | After failure | Non-critical assets where failure has limited impact | Creates unplanned work and can extend production interruptions |
Preventive | At fixed time or usage intervals | Known age- or usage-related failure patterns | May service healthy components and cannot address random failures reliably |
Condition-based | When measured condition deviates | Assets with measurable health indicators and defined thresholds | Requires suitable sensing, baselines, and response rules |
Predictive | Before a forecast failure | Critical assets with sufficient history, context, and analytical capability | Depends on data quality, relevant models, and operational follow-through |
What is condition monitoring in a packaging machine?
Condition monitoring is the continuous or periodic measurement and evaluation of machine-health indicators to identify changes from normal operation. Depending on the component and failure mode, relevant data can include vibration, temperature, pressure, flow, current, humidity, operating hours, or process values.
The objective is not to collect as much data as possible. It is to detect meaningful deviations early enough for a maintenance team to investigate, plan work, and avoid an unexpected stop. A useful monitoring concept therefore links each measurement to a component, a likely failure mode, an alert rule, and a defined action.
What is the difference between condition monitoring and predictive maintenance?
Condition monitoring describes the current state of an asset and flags abnormal behavior. Predictive maintenance builds on condition data, operating history, and analytics to estimate how a fault may develop and when intervention may be required.
In practice, OEMs should establish reliable measurements and meaningful condition-based alerts before making predictive claims. A stable baseline, relevant operating context, and feedback from completed maintenance actions make subsequent trend analysis more useful.
Where does monitoring create the most value in packaging machinery?
The strongest candidates are critical components whose failure would stop production, impair quality, or require costly troubleshooting. Typical examples include rotating assets such as motors, gearboxes, bearings, pumps, and fans, along with pneumatic systems and sensors that are essential to process control.
Selection should be risk-based rather than portfolio-based. OEMs can prioritize monitoring points by asking: What happens if this component fails? Is deterioration measurable? Is there enough time to act after an alert? Can the service team identify a specific response?
What are the broader benefits for packaging OEMs?
While condition monitoring is often associated with maintenance, its impact extends beyond service activities. When considered during machine design, it can support commissioning, simplify troubleshooting, improve machine transparency, and contribute to more standardized machine architectures.
Technical benefits | Operational benefits | Business benefits |
Easier commissioning and troubleshooting | Improved machine availability | Higher OEE |
Better understanding of machine behavior in real operating conditions | Reduced service effort | Lower total cost of ownership (TCO) |
Easier integration into standardized machine architectures | Fewer unplanned interventions | Increased reliability of delivered machines |
For OEMs, these benefits can influence not only maintenance outcomes, but also machine design decisions, lifecycle support strategies, and overall machine performance.
Monitoring technologies should be selected based on the failure modes that need to be detected and the available response time.
Vibration can reveal changes associated with wear, imbalance, misalignment, looseness, or gear defects in rotating equipment.
Temperature can indicate overheating, friction, or lubrication-related problems.
Pressure and flow can help reveal leaks, restrictions, or declining performance in pneumatic and fluid systems.
Operating hours and process values provide context for interpreting changes under different machine states.
How does condition monitoring support OEE?
Condition monitoring primarily supports the availability component of OEE by helping teams detect developing issues and plan maintenance before an unexpected failure. It can also support performance and quality when the monitored condition affects cycle stability, positioning, pressure, temperature, or another process-critical parameter.
Monitoring does not improve OEE automatically. The improvement depends on whether alerts are relevant, responsibilities are clear, maintenance can act in time, and the organization tracks whether interventions prevent recurring losses.
How should OEMs integrate condition monitoring?
A scalable design starts with the maintenance decision and works backward to the data source. For OEMs, the challenge is often not collecting more data but integrating condition information into a scalable machine architecture where alerts and insights support real maintenance decisions. This prevents a technically impressive monitoring layer from becoming additional complexity without operational value.
Define the critical asset and failure consequence. Focus first on components that materially affect availability, quality, safety, or repair effort.
Choose a measurable indicator. Match vibration, temperature, pressure, or another parameter to the expected failure mode.
Capture operating context. Distinguish normal variation caused by speed, load, format, recipe, or machine state from genuine deterioration.
Set baselines, thresholds, and escalation rules. Specify who receives an alert, what must be checked, and how urgent the response is.
Use standardized communication and accessible data. Make condition information available to the people and systems that need it without unnecessary architecture changes.
Validate and improve. Compare alerts with inspections and completed repairs, then refine thresholds and monitoring tasks.
How Balluff supports a scalable monitoring architecture
Balluff combines sensing, communication, and data evaluation in a modular condition-monitoring approach. Condition-monitoring sensors provide measurements such as vibration, temperature, and pressure. IO-Link supports standardized device communication and simplifies the integration of condition-monitoring devices across machine architectures, while the Condition Monitoring Toolkit (CMTK) combines hardware and software for automated data acquisition, evaluation, visualization, and configurable notifications.
The CMTK can operate independently of existing IT and automation networks, and it can provide data through OPC UA and MQTT for use in local networks or cloud systems. Balluff also states that connected IO-Link sensors can collect condition data without adapting the existing system. The BCM Assistant supports configuration of Balluff condition-monitoring sensors for specific applications and monitoring functions.
For packaging OEMs, the architectural benefit is a clearer path from measurement to maintenance action: appropriate sensors capture machine condition, standardized communication transports the data, and the monitoring layer turns deviations into visible information and alerts. The final design still needs to account for the machine’s risks, operating states, hygiene requirements, control environment, and service process.
From maintenance feature to machine-performance strategy
Condition monitoring becomes most valuable when it is designed into the machine lifecycle rather than added as an isolated sensor package. It can support commissioning by making abnormal behavior visible, accelerate root-cause analysis during startup and ramp-up, improve service diagnostics through historical condition data, and give end users a clearer basis for maintenance planning.
The goal is not more data, but actionable insight that makes machine condition easier to understand and maintenance decisions easier to plan. For OEMs, that can strengthen reliability, lifecycle transparency, and differentiation in applications where uptime is a decisive buying criterion.
Takeaways
Use condition monitoring to make relevant changes in machine health visible before they become production interruptions.
Distinguish current-state monitoring from predictive maintenance; prediction requires reliable data, context, history, and validated analytics.
Prioritize components by failure consequence, measurability, warning time, and the availability of a clear maintenance response.
Integrate sensing, communication, alerts, and service workflows as one architecture rather than as separate technology projects.
Evaluate success through avoided failures, actionable alerts, maintenance response, and the resulting effect on machine availability and OEE.
Frequently asked questions
Can condition monitoring be retrofitted to existing packaging machines?
Yes, retrofit is possible when suitable mounting points, power, communication, and access to the relevant machine components are available. A retrofit assessment should begin with critical assets and the maintenance decisions the system must support. Balluff positions the CMTK as a control-independent solution that can work alongside existing automation networks.
Does condition monitoring replace preventive maintenance?
No. Condition monitoring complements preventive maintenance by adding evidence about actual machine condition. Fixed-interval tasks may still be appropriate for safety requirements, consumables, inspections, or components with known age-related wear.
Which measurement should an OEM start with?
Start with the failure mode, not the sensor. Use vibration for many rotating mechanical issues, temperature for thermal changes, and pressure or flow for pneumatic and fluid-system behavior. The correct choice depends on what deterioration must be detected and how early action is possible.
Is predictive maintenance the same as an alarm limit?
No. A limit alarm indicates that a current value or derived condition has crossed a defined threshold. Predictive maintenance uses condition trends, operating context, history, and analytics to estimate future failure or remaining time to intervention.
What determines whether a monitoring project improves OEE?
The project must produce timely, trustworthy, and actionable information. Clear ownership, suitable thresholds, prepared maintenance responses, and validation against real inspections or repairs are as important as the sensing technology.
Keywords
- Condition Monitoring
- Verpackungsindustrie
Author
Roberto Caffarelli
12 Contributions
Comment
Popular posts
An easy way to remember PNP and NPN sensor wiring
Real-time speed of IO-Link wired
Advantages of inductive proximity sensors in industry
Automation for intralogistics: a practical perspective
Contact form
Do you have any questions or suggestions? We are at your disposal.
Balluff GmbH
-
Zabergäustraße 8
73765 Neuhausen a.d.F.