Products
Service & Support
Industries & Solutions
Company

How to select the best lighting techniques for your machine vision application

Learn the seven main lighting techniques for machine vision applications, focusing on image stability through lighting, lensing, and material handling

Balluff Editor
01 Mar 2024 | 23:25 Clock

Reading Time: minutes

The key to deploying a robust machine vision application in a factory automation setting is ensuring you create the environment for a stable image. The three areas you must focus on to ensure image stability are lighting, lensing, and material handling. For this blog, I will focus on the seven main lighting techniques used in machine vision applications.

On-axis ring lighting

On-axis ring lighting is the most common type of lighting because, in many cases, it is integrated on the camera and available as one part number. When using this type of lighting, you almost always want to be a few degrees off perpendicular (Image 1A).  If you are perpendicular to the object, you will get hot spots in the image (Image 1B), which is undesirable. When the camera with its ring light is tilted slightly off perpendicular you achieve the desired image (Image 1C).

Image 1A

Image 1B

Image 1C

Off-axis bright field lighting

Off-axis bright field lighting works by having a separate LED source mounted at about 15 degrees off perpendicular and having the camera mounted perpendicular to the surface (Image 2A). This lighting technique works best on mostly flat surfaces. The main surface or field will be bright, and the holes or indentations will be dark (Image 2B).

Image 2A

Image 2B

Dark field lighting

Dark field lighting is required to be very close to the part, usually within an inch. The mounting angle of the dark field LEDs needs to be at least 45 degrees or more to create the desired effect (Image 3A).  In short, it has the opposite effect of Bright Field lighting, meaning the surface or field is dark, and the indentations or bumps will be much brighter (Image 3B).

Image 3A

Image 3B

Backlighting

Backlighting works by having the camera pointed directly at the backlight in a perpendicular mount. The object you are inspecting is positioned between the camera and the backlight (Image 4A). This lighting technique is the most robust because it creates a black target on a white background (Image 4B).

Image 4A

Image 4B

Diffused dome lighting

Diffused dome lighting, aka the salad bowl light, works by having a hole at the top of the salad bowl where the camera is mounted and the LEDs are mounted down at the rim of the salad bowl, pointing straight up, which causes the light to reflect off of the curved surface of the salad bowl. It creates a very uniform reflection (Image 5A).  Diffused dome lighting is used when the object you are inspecting is curved or non-uniform (Image 5B). After applying this lighting technique to an uneven surface or texture, hotspots, and other sharp details are deemphasized, creating a matte finish to the image (Image 5C).

Image 5A

Image 5B

Image 5C

Diffused on-axis lighting

Diffused on-axis lighting, or DOAL, works by having a LED light source pointed at a beam splitter. The reflected light is then parallel with the direction in which the camera is mounted (Image 6A). DOAL lighting should only be used on flat surfaces where you are trying to diminish very shiny parts of the surface to create a uniform image. Applications like DVD, CD, or silicon wafer inspection are some of the most common uses for this type of lighting.

Image 6A

Structured laser line lighting

Structured laser line lighting works by projecting a laser line onto a three-dimensional object (Image 7A), resulting in an image that gives information on the object's height. Depending on the mounting angle of the camera and laser line transmitter, the resulting laser line shift will be larger or smaller as you change the angle of the devices (Image 7B). When there is no object, the laser line will be flat (Image 7C).

Image 7A

Image 7B

Image 7C

Real-life applications  

The images below, (Image 8A) and (Image 8B), were used for an application that requires counting the pins of a connector. As you can see, the bright field lighting on the left does not produce a clear image, but the dark field lighting on the right does.

Image 8A

Image 8B

This next example (Image 9A) and (Image 9B) was for an application requiring a bar code read through a cellophane wrapper. The unclear image (Image 9A) was acquired using an on-axis ring light, while dome lighting (Image 9B) resulted in a clear, easy-to-read image of the bar code.

Image 9A

Image 9B

This example (Image 10A), (Image 10B), and (Image 10C) highlight different lighting techniques on the same object. In the (Image 10A) image, backlighting is used to measure the smaller hole diameter. In the image (Image 10B), dome lighting is used to inspect the upper hole's taper in reference to the lower hole. In (Image 10C) dark field lighting is used for optical character recognition “OCR” on the object. Each of these could be viewed as positive or negative, depending on your goal.

Image 10A

Image 10B

Image 10C

Keywords

  • Machine vision

Did you like this post?

2

Share this post

Author

Balluff Editor


9 Contributions

Comment

Discover related topics

Energy consumption labeling
Energy consumption labeling

EPREL - European Product Database for Energy Labeling

For all questions concerning commercial topics such as quotations, orders, and delivery times, our inside sales department will be happy to support you: [email protected]
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
In order to add a free sample product to the cart we will need to remove all the normal products from the cart. Are you sure you want to continue